Chinese  |  Group Corporate Site  |  Search

  China
Our Company
Energy Business
Telecom Business
People & Careers
Home    Telecom Business: Sirocco Blown Fibre    Products    Optical Fibre
Solutions for your Business
Optical Fibres
Optical Cable
Communications Copper Cables
FTTx Passive Solutions
Sirocco Blown Fibre
Applications
News & Views
Products
Optical Fibre
Blown Fibre Units
Blown Fibre Tube Cable
Installation Equipment
Accessories
External Plant
Internal Plant
Cost Savings
Features & Benefits
Services
OPGW System
OAsys® Connectivity
Deskwave Premises
News Archive
Events
Optical Fibre

Prysmian is one of the world's largest producers of high quality, high performance optical fibre. These products range from long distance submarine grade fibres (DeepLight) and terrestrial fibres (FreeLight and WideLight) meeting ITU-T G.655 requirements, to short haul fibres for access and premise networks. It is these latter fibres that are used in Sirocco.

The datasheets accessible below identify the optical and geometric properties of the various fibre types used in the manufacture of the Prysmian range of Sirocco fibre bundles. If you require more information about the performance of Prysmian optical fibres please contact us .

• Singlemode Fibre
The Optical Fibre that sets Standards
Standard singlemode optical fibres are most suitable for the 1310nm wavelength range, but can also be used at 1550nm. This allows singlemode fibre to be used with a variety of sources, from LED's to lasers, offering a highly versatile fibre carrying high bit rates on multiple channels. Prysmian singlemode fibre is compatible with other fibres and employed across the world in optical systems.

• MagniLight Fibre
Low water peak singlemode fibre offers the possibility of extra bandwidth (65% more usable wavelengths) by reducing the water peak around 1383 nm enabling it to be used with current and emerging technologies that can reduce network costs by increasing transmission capacity.

 
• Multimode Fibre
The best solution for local applications.
Multimode fibres are intended for all applications where the distances covered are short, such as Local Area Networks (LAN) or all networks with a small reach like campus, buildings or offices. A multimode fibre also enables connections for backbone, riser and horizontal links. All these networks are characterised as having many points of access to the fibre and the short distances covered. The index profile of multimode fibres is specifically tuned to provide the optimum solution for these local applications.
The range of multimode fibres has been extended over the last few years in order to offer solutions for 10 Gbit operation. Prysmian now manufactures Sirocco fibre bundles with four options of multimode fibre.

Prysmian fibres are manufactured using Neon technology, where a coloured layer of acrylate is applied to the fibre during drawing instead of adding an inked layer afterwards. The advantages offered by this technology include:

• Improved watersoak performance, fibres have been immersed in water for almost 10-years with no sign of degradation
• Better control of finished fibre dimensions, particularly valuable in ribbon fibres
• More lucid, vibrant colours for easy differentiation when splicing

Site Map  |  Legal Information  |   Company info  |  Copyright © 2012 All rights reserved.