Chinese  |  Group Corporate Site  |  Search

  China
Our Company
Energy Business
Telecom Business
People & Careers
Home    Telecom Business: Optical Fibres    SM Light
Solutions for your Business
Optical Fibres
CasaLight™ Fibre
FreeLight™ Fibre
WideLight™
SM Light
DeepLight™ Fibre
MagniLight™ Fibre
FineLight™ Fibre
Multimode fibres 50/125
Multimode fibres 62.5/125
Optical Cable
Communications Copper Cables
FTTx Passive Solutions
Sirocco Blown Fibre
OPGW System
OAsys® Connectivity
Deskwave Premises
News Archive
Events
SM Light

Introduction
Single mode fibres still account for the great majority, by volume, of fibre installed every year in the world.

• High Bandwidth
Single mode optical fibres are best suited for the 1310 nm wavelength range, but can also be used around 1550 nm. To this purpose, SM Light is fully characterized through to 1625 nm, permitting the transmission of multiple channels over long distances.

• Compatibility
Single mode optical fibres are at the core of the majority of installations throughout the world. A vast database has been accumulated over time that shows this fibre to be a truly compatible product, both with other fibres and with optical systems employed globally.

• PMD Excellence
SM Light still sets the PMD world standard for ITU-T G.652 fibres, a parameter where only true excellence allows achieving such low value.

• Fibre Coating
SM Light is also available with the latest generation coating: Neon™Plus. Neon™Plus is an evolution of the highly acclaimed Neon™ coating used by Prysmian worldwide for well over 10 years. This coating offers increased resistance to bending and improved performances against temperature variation and mechanical disturbances.

Download the brochure  


Site Map  |  Legal Information  |   Company info  |  Copyright © 2012 All rights reserved.